DRV.CUSTOMIDENTIFIER

Description

Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:

  • ASCII characters only
  • 32 character max length
  • No spaces in string

The string is displayed on the device overview screen and in the start page's device discovery table.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

-

Data Type

String

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DRV.CUSTOMIDENTIFIER

2010

7DA

String

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.CUSTOMIDENTIFIER

2010

String

Read/Write

-